Hi!
I tried to make my own “bq51013AEVM-765 Evaluation Module”, but it doesn’t work. I used the same schematic as in the evaluation module and tried to use the same layout.
When I connect the transmitter to 5V, one LED lights up and there is a short signal on the coil every 400ms. But the receiver does nothing. There is no output voltage, or other signals.
When I tried to check the receiver, I connected 5V to the “J1 – AD External Adapter Input, J2-GND” pins. But nothing happened. The LED doesn’t light up. There is no signal to the MOSFETS.
I don’t know what’s wrong. Could it be the IC? Is it better to replace the BQ51013A with the BQ51013B?
Thanks and best regards,
Philipp