This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54620 PVIN lower than Vin

Other Parts Discussed in Thread: TPS54620

Hello

I wanted to design a TPS54620 supply for 12V Vin=PVin to 1 V with 5A running at 600kHz  on a board with high temperatures up to 70 degree C.

Simulations with Switcherpro and Webench showed a  to high temperatur on the device.

With an input voltage of 5V the power dissipation and hence the temperature of the device is reduced.

I expect that a split input rail with Vin = 12V and PVin = 3.3V would reduce the temperature of the device even more.

How can I simulate or calculate such an design?

Regards

Reiner Boettcher