One of my customers is having problems with the TPS54620.
12V to 5V 5A
The TPS54620 is randomly dying in short circuit (I think it closes both top and bottom MOSFET at the same time, then overcurrent latch them up), after a while it delivers around 10V (I think it is when the bottom side MOSFET dies).
I attached the schematics for this design.
We found a workaround for now, but we need to understand what is happening.
The workaround is to remove FB14.
The customer wants to understand why this phenomenon is happening, and what to do against it.
Johan1781.POWER.PDF