This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQEasy command line

Other Parts Discussed in Thread: BQ27510

Hi, I am using bqeasy to talk to a bq27510 and I can successfully read and write the data flash.  I have exported the data flash and can successfully import it.  Now, I would like to do this in an automated fashion.  Is there a command line interface to bqeasy?  Or is there a similar tool that does have a command line interface?  I would like to connect to a device and export a stored data flash file, then "write all" without having to click the buttons.  Thanks for the help.