Hey,
So I'm a little overwhelmed with all of TI's options for boost converters, can you guys please point me in the rite direction please?
I'm going to be giving it 3.0v - 4.2v, and the output should be variable, in increments of .1v, up to 6v. The battery can support up to 15amps drain, and I'm looking to get somewhere around 40watts consistent output. I'd like to use a digital pot, but if I need to use something that's set up for an analog one, and convert it, that's not a huge problem.
Ideally, the Boost Converter should have <80% efficiency.
Please let me know if I'm posting this in the wrong place, I don't know the difference between isolated DC/DC converters, and non-isolated ones.
Thanks for the help.