I have application that requires multiple bq27520G3 chips for multiple sub-system, may I tie all SCL, SDO together with common pull-up? Since there is no address information encoded in bq27520G3 chip, so I will use CE to select the individual bq27520G3 to read/write data from SCL, SDO. Will this cause any contention problem from the un-selected bq27520G3 chip?
I know that VCC will be dropped to 0V when CE=0, and I assume that VCC is the supply of whole chip, so the SCL, SDO will be in Z-state when CE=0, so it will not cause contention problem to the selected SCL, SDO operation. If this is not right, please advise the solution.
Thanks a lot.
Chuck Hung 10/25/13