Dear Sir:
company ASKEY currently has encountered a phenomenon, when the battery voltage is 4.0v or more, Setting the charging voltage from 4.2v change to 4.0v, Setting the charging current from 0.96A change to 0.57A.Readind reg: 08 of bit4, 5 shows a display like this should be ''10 - Fast Charging'', change to "11 - Charge Termination Done" But we found that it sometimes reads Back to 00 - Not Charging. So if we transform before charging voltage and current,
need disable charger and then set reg02 reg04 then enable to start charging?