Hi.
Please tell me about the following equation.
(TPS54233 data sheet P13 OUTPUT FILTER COMPONENTS 「Capacitor Selection」 )
"D" Is it Duty?
What do you mean by "D-0.5"?
Please explain equation.
Regards,
Yusuke Tsukui.
Yusuke Tsukui.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I vaguely remember about this. The ripple voltage on the output has two primary components, the part due to the ripple current thru the ESR of the output caps and the part due to charging and discharging the capacitance. They are not in phase with each other. D is in fact the duty cycle. For D less than 50%, the effect may be subtractive. it is a long time since I have seen this derived, but I am pretty sure it is correct.