Hi,
Can I use the LMZ30606 (or LMZ30604) with only ceramic capacitors at the output?
For example:
For 1.2V output, TI suggest to use 47uF ceramic + 330uF POSCAP. I like to use 4x 100uF, X5R, 6.3V, 1206 ceramic capacitors instead.
By-the-way - the schematics shown in the EVB datasheet is very blurry...
Thanks,
Noam