hello Al,
My question is related to the TPS54618 and, in general, to any DC/DC switcher:
There is a clear path inside the TPS54618 from the EN pin input, through the Shutdown internal signal (see functional block diagram) and to the high/low end FETs' gates (internal FETs that connect to the PH pin).
This path includes amplifiers and logic.
I require the min/max timing from an EN disable strobe and until a proper strobe appears in FETs' gates (the FETs that connect internally to the PH pin).
Thank you
Gil Hershman