Hello,
We need DCDC converter with below three functions.
-CV
-CC
-Output current is limited when Input voltage is decreased functions.
Please see the attached file as CC,CV circuit.
And please let me know the below questions.
(1) Can we use this circuit with TPS40304?
(2) We want to add the function that If Input voltage is decreased , output current is limited.
Can we add the this function to TPS40304 by optional circuit.
(for example, add the EA to above circuit)
If TPS40304 can’t , please let me know the other device.
I think that bq24650 may operate above function.
Can we add the this function to TPS40304 by optional circuit.
(for example, add the EA to above circuit)
If TPS40304 can’t , please let me know the other device.
I think that bq24650 may operate above function.
Best Regards,
Ryuji Asaka