Hello,
I'm having an issue polling data from a bq78PL116. I'm checking the status via command 0x80, and only requesting data after the response is 0x0000.
The application works fine, I poll data every second or so......for a minute or two, then i get a NACK from the BMS on the address 0x16.
The resultant data from issuing command 0x80 is also not matching anything in Table 2 of SLUA591.
Are there any things i must address such as timing, permeable bytes.....any tips would help.
Im using a beagle I2C sniffer.
Thanks in advance.
BRuce