We’re currently using the TI BQ27541-V200 battery fuel gauge but I would like to explore other options for something that is simpler to setup. Currently we’re using a golden image, then we have to calibrate the gauge to the specific cell that we’re going to use in the system. It would be nice if we didn’t have to do the cal process, and instead just program a few registers with new cell capacity, voltage, number of cells, and chemistry. I’d be willing to sacrifice some accuracy if we could simplify the setup.
Any thoughts on parts that might be better for our application? It’d be nice to retain the impedance track feature.