This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ua7805, input and output capacitor

Hi all,

I'd like to use the ua7805 in my current project. Input voltage should be between 7V and 15V. Output current should be 400mA at max. Since I have the following two caps already available I'd like to know if they will do their job because the caps indicated in the datasheet of the regulator have a far smaller cap value (0.33uF for the input and 0.1uF for the output):

Input: Vishay Cap, Tantal, SMD TR3B, 20V 10uF
Output: Vishay Cap, Tantal, SMD 293D, 16V 10uF

Thank you for your help and advice

Christian