This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ51013B drops the power

Other Parts Discussed in Thread: BQ51013B

Hi,

I have the receiver with BQ51013B and connected two my phone using USB connection. Every 30 sec or so it will drop the power and the TX shuts down for 1 sec and then reconnects. 

This happens more when the battery power on the phone is above 70%, It also happens when the battery is less but the frequency of shutdown is less. 

I think the RX is sending out charge full communication to TX. I have grounded EN1 and EN2 pin and still it is happening. Please help. 

Regards,

Bency