I created a PCB using the TPS54386 chip. I designed my circuit using the Switcher Pro application as a resource. In my circuit, Vin is 24V and the outputs are 12V and 5V. I powered the circuit at first without a load connected. When doing this, the voltages were correct. Next I tried to power a Beaglebone using the 5V output. When attempting this the TPS54386 caught on fire. When examining the damaged IC, it looks as though the damage occurred around the Analog Ground, EN1 and EN2 pins on the chip. Any suggestions?
As a side note, when removing the chip, it may have been possible that the PowerPad was making contact but not soldered fully to the ground trace/plane. Could this have caused an issue? The Beaglebone is still functional.