Hi
Like to check on the BQ24295.
After the DCD and primary detection process. If there is no standard charger detected, the DCD timer of 0.5Sec would lapse and enter into "non-standard charger detection phase".
Based on the values of the DPDM, the corresponding current limit is set according to table 3 of datasheet.
The main objective, I would like to set a limit of 500mA on the current limit regardless of the values detected on the DPDM during/before the "non-standard charger detection phase". ie,even if there is a divider 1 type (table 3), instead of setting 2A, i want 0.5A
A few questions:
- Can i interrupt or terminate the non-standard charger detection phase and set my own current limit?
- For the USB 1.2 detection phase, what is the time needed to determine the source and set the (REG00[2:0] to either 01 or 10?
Lastly, if I plan is to read the value of REG08[7:6] at 0.4Sec, and the value readback is still 00, I would write 010 to REG0[2:0]. Will it work?
Ivan