This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS5450 blows up

Other Parts Discussed in Thread: TPS5450

I'm using a TPA5450 for generate a 5V starting from a 24VDC.In my board the load absorbs 3A; I'm already in production with it and the design seems ok, but in few boards (about 3-4%) the chip blows up at the first power-up or after few minutes, also with a load less then 3A. I see that the component is shorted towards ground at pin 8 (PH).

What could be happen?

Is this component thermal protected?

regards

Luca