Hi,
I am working with a TPS2491DGS as a 48V power supply hot swap controller. I am finding that the chip reference voltage on pin 2 is about 1.2V instead of 4V. VCC at pin 10 is 47.5V and Enable at pin 1 is 3.3V. I have used many chips and the result is the same. I have also separated pin 2 from the PCB the pin and Vref is still 1.2V.
Can the connection from the sense resistor to the IC affect the reference voltage on pin 2 ?
Thank you.
Shahram