This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24650EVM charge current

I have tried to use the above mentioned EVM for charging a 12.6 V battery which is discharged to 11.5 V in the starting.

i observed that voltage at the output of the EVM was as mentioned 12.6 V but the current in circuit was almost 0 Amp.

please tell me the possible reasons. i have also tried to connect the above EVM from two different power sources and i got the same results.

i.e current is not flowing into the circuit. Whereas as per factory setting i should see 0.2 Amp in starting which becomes 2 Amps after 30 mins.

Thanks