This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Device latchup



What is device latchup. If an IC like 7660 is latched up, is it permanently broken? Or it can be reset?

  • Dear Rani,

    A latchup is a type of short circuit, normally occurs in an improperly designed IC. As we know in CMOS technology, there are a number of instrinsic BJT, and in CMOS processes, these BJTs may create problems when the combination between n-well and p-well andsubstrate rsults in the formation of parasitic n-p-n-p structures.If these  parasitic structure are triggered which will lead to a short of the Vdd and GND lines, usually resulting in destruction of the chip, or a system failure that can only be resolved by power-down

    The figure below is a schematic about parasistic transistors in a CMOS circuit. A p-n-p-n structure acts as a PNP and an NPN transistor stacled next to each other. During a latchup, when one of the transistor is conducting, the other one begins conduction as well. They keep each other in saturation for as long as the structure is forward-biased and some current flows through it, that normally means until a power-down.

    The latchup can happen at any place where the required parasitic structure exists. The causes of latchup are multiple, a spike of positive or negative voltage on an input or output pin, or the supply voltage exceeding the absolute maximum ration etc.

    The link below is a TI Application Note about latchup:

    http://www.ti.com/general/docs/lit/getliterature.tsp?baseLiteratureNumber=SLYA014&fileType=pdf

     

    Talking about whether a latchup will cause a permanent broken-down to a device, I think it's hard to say. It depands on whether latchup is just causing a simple short or damages some electronic elements. You can try to re- power the device for making sure whether it can be recovered.

    Best Regards

    Na