Hi folks,
for the supply of an H-bridge (for a galvanometer) I've chosen the TPS54540. Vin = 24V, Vout+15V Ioutmax= 3A. This works wonderful with a static load, even at 3A the switcher doesn't get too hot.
But with a switched load it doesn't look that nice. When the load (5R) is switched on, Uout is still 15V after a short drop to 13V. When the load is taken off, Uout is ~16V.
Here some data:
Cin = 2* 4.7µ ceramic
Cout = 3* 22µ ceramic
Fsw = 400KHz
L = 22µH
Rcomp = 10K
ccomp = 22n
Anyone has an idea?
:-) Sarah