Problem:
The chip keeps reverting into the shutdown mode, but I have checked for all of the faults modes (OV, UV, OCD, SCD, SCC, OT, etc.) and do not see anything wrong. I would like to be able to read out an error code of some kind to tell me what is causing shutdown mode.
Background:
I have been working on a project that can be powered by a 4-cell LiPo battery pack or by an 18V wall adapter, and will recharge the battery when both are connected. I am using the BQ77908A to protect the battery, and I am using the "4- to 8-Series Cell Configuration" on p. 37 of the datasheet.
Any help would be much appreciated :)