Hi All,
I need a topology/device advice for a DC-DC Converter, to be used in harsh industrial environment with the following spec:
- Input 50V DC to 175V DC
- Isolated Output 1 : 110VDC - 3Amps - Peak 4.5Amps (A number of 110V DC Contactor Coils as load)
- Isolated Output 2 : 24V DC / 2Amps Max
The load is varying in nature and may vary from 10% to 100%. Key concerns are efficiency, robustness, board-space.
I am basically a programmer with exposure in power electronics and would always consider myself a SMPS newbie, so I need pointers before proceeding.
Regards
Sougata