This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

NEED INFORMATION- LMR64010XMF/NOPB

Hi Can you please provide the following information for the PTN0805E6811BST1 Part ?

1. Junction Temperature Max (Tj Max)

 2. Typical Power dissipation (Pd typ)

3. Maximum Power dissipation (Pd max)

4. Thermal Resistance Junction to Ambient (Theta JA

5. Thermal Resistance Junction to Board (Theta JB)

6. Thermal Resistance Junction to Case (Theta JC)

7. Weight

  • Hi Jayakumara,

    1. Junction Temperature Max (Tj Max) - 125C operating, 150C Abs Max

     2. Typical Power dissipation (Pd typ) - Depends on application

    3. Maximum Power dissipation (Pd max) - 265mW

    4. Thermal Resistance Junction to Ambient (Theta JA) - 265C/W

    5. Thermal Resistance Junction to Board (Theta JB) - Not spec'd

    6. Thermal Resistance Junction to Case (Theta JC) - 60C/W

    7. Weight - Not Spec'd.

    Thanks,

    Anston