Hi
hope someone can please give me a few pointers.
my config is a 4 serial x 2 parallel LION battery of 4500mAh. my max voltage is 16.8 volts when charging.
I have been for many long days now trying to complete the learning Algorithm for the bq34z100. I can get the update status to get to 5 but no matter how many times i try it never goes to 6.
here is the process i'm following as given by Tom from a previous post.
Set your Flash Update OK voltage to 2000mV. Set the FConvEn bit to 0 in the Pack Cfg B register.
1. Send an IT Enable (21) command to turn ON FETs. Send a Reset command (41) to disable Ra-table updates.
2. Discharge to empty
3. Wait until the OCVTAKEN flag turns red.
4. Send IT Enable command to set a DOD0 reference point.
5. Charge to full (FC bit set.)
6. Wait until the OCVTAKEN flag turns red. You should see VOK turn green after Qmax has learned. You should see Update Status change to a 05.
7. Discharge at a C/8 rate down to Term Voltage.
8. Wait until the OCVTAKEN flag turns red. You should see Update Status change to a 06 during the rest period.
if the process fails at what point in the list do i start the process again. I have been reloading the senc file and calibrating the board. but if theres a better way of trying the algorithm again could you decribe it please.
i would great appreciate some pointers to where i'm going wrong.
attached is the .gg file of my config and current state.
[Header] bq EVSW Version = 0.9.90 DeviceName = bq34z100 v0.06 Time = 14/11/2013 09:37:09 [Safety(Configuration)] OT Chg = 55.0 OT Chg Time = 2 OT Chg Recovery = 50.0 OT Dsg = 60.0 OT Dsg Time = 2 OT Dsg Recovery = 55.0 [Charge Inhibit Cfg(Configuration)] Chg Inhibit Temp Low = 0.0 Chg Inhibit Temp High = 45.0 Temp Hys = 5.0 [Charge(Configuration)] Suspend Low Temp = -5.0 Suspend High Temp = 55.0 [Charge Termination(Configuration)] Taper Current = 100 Min Taper Capacity = 25 Cell Taper Voltage = 100 Current Taper Window = 40 TCA Set % = 99 TCA Clear % = 95 FC Set % = 100 FC Clear % = 98 DODatEOC Delta T = 10.0 [Data(Configuration)] Rem Cap Alarm = 100 Initial Standby = -10 Initial MaxLoad = -500 Manuf Date = 01-Jan-1980 Ser. Num. = 0102 Cycle Count = 2 CC Threshold = 4050 Design Capacity = 4500 Design Energy = 16200 SOH Load I = -400 TDD SOH Percent = 90 Cell Charge Voltage T1-T2 = 4200 Cell Charge Voltage T2-T3 = 4200 Cell Charge Voltage T3-T4 = 4100 Charge Current T1-T2 = 10 Charge Current T2-T3 = 50 Charge Current T3-T4 = 30 JEITA T1 = 0 JEITA T2 = 10 JEITA T3 = 45 JEITA T4 = 55 ISD Current = 10 ISD I Filter = 127 Min ISD Time = 7 Design Energy Scale = 1 Device Name = bq34z100 Manufacturer Name = Texas Inst. Device Chemistry = LION [Discharge(Configuration)] SOC1 Set Threshold = 150 SOC1 Clear Threshold = 175 SOCF Set Threshold = 75 SOCF Clear Threshold = 100 Cell BL Set Volt Threshold = 2800 Cell BL Set Volt Time = 2 Cell BL Clear Volt Threshold = 2900 Cell BH Set Volt Threshold = 4300 Cell BH Volt Time = 2 Cell BH Clear Volt Threshold = 4200 [Manufacturer Data(Configuration)] Pack Lot Code = 0000 PCB Lot Code = 0000 Firmware Version = 0000 Hardware Revision = 0000 Cell Revision = 0000 DF Config Version = 0000 [Integrity Data(Configuration)] Static Chem DF Checksum = 7D9F [Lifetime Data(Configuration)] Lifetime Max Temp = 32.3 Lifetime Min Temp = -39.2 Lifetime Max Chg Current = 1976 Lifetime Max Dsg Current = -649 Lifetime Max Pack Voltage = 16784 Lifetime Min Pack Voltage = 3500 [Lifetime Temp Samples(Configuration)] LT Flash Cnt = 36 [Registers(Configuration)] Pack Configuration = 0940 Pack Configuration B = FE Pack Configuration C = 30 LED_Comm Configuration = 00 Alert Configuration = 0000 Number of series cell = 4 [Lifetime Resolution(Configuration)] LT Temp Res = 1.0 LT Cur Res = 100 LT V Res = 25 LT Update Time = 60 [LED Display(Configuration)] LED Hold Time = 4 [Power(Configuration)] Flash Update OK Cell Volt = 2000 Sleep Current = 10 FS Wait = 0 [Manufacturer Info(System Data)] Block A 0 = 00 Block A 1 = 00 Block A 2 = 00 Block A 3 = 00 Block A 4 = 00 Block A 5 = 00 Block A 6 = 00 Block A 7 = 00 Block A 8 = 00 Block A 9 = 00 Block A 10 = 00 Block A 11 = 00 Block A 12 = 00 Block A 13 = 00 Block A 14 = 00 Block A 15 = 00 Block A 16 = 00 Block A 17 = 00 Block A 18 = 00 Block A 19 = 00 Block A 20 = 00 Block A 21 = 00 Block A 22 = 00 Block A 23 = 00 Block A 24 = 00 Block A 25 = 00 Block A 26 = 00 Block A 27 = 00 Block A 28 = 00 Block A 29 = 00 Block A 30 = 00 Block A 31 = 00 [IT Cfg(Gas Gauging)] Load Select = 1 Load Mode = 0 Max Res Factor = 15 Min Res Factor = 3 Ra Filter = 500 Fast Qmax Start DOD % = 92 Fast Qmax End DOD % = 96 Fast Qmax Start Volt Delta = 200 Cell Terminate Voltage = 3300 Cell Term V Delta = 50 ResRelax Time = 200 User Rate-mA = 0 User Rate-Pwr = 0 Reserve Cap-mAh = 0 Reserve Energy = 0 Max Scale Back Grid = 4 Cell Max DeltaV = 200 Cell Min DeltaV = 0 Max Sim Rate = 2 Min Sim Rate = 20 Ra Max Delta = 44 Qmax Max Delta % = 5 Cell DeltaV Max Delta = 10 Fast Scale Start SOC = 10 Charge Hys V Shift = 40 [Current Thresholds(Gas Gauging)] Dsg Current Threshold = 60 Chg Current Threshold = 75 Quit Current = 40 Dsg Relax Time = 60 Chg Relax Time = 60 Quit Relax Time = 1 Cell Max IR Correct = 400 [State(Gas Gauging)] Qmax Cell 0 = 4690 Cycle Count = 1 Update Status = 05 Cell V at Chg Term = 4195 Avg I Last Run = -299 Avg P Last Run = -1131 Cell Delta Voltage = 2 T Rise = 20 T Time Constant = 1000 [OCVa Table(OCV Table)] Chem ID = 0100 [R_a0(Ra Table)] Cell0 R_a flag = FF55 Cell0 R_a 0 = 38 Cell0 R_a 1 = 41 Cell0 R_a 2 = 43 Cell0 R_a 3 = 44 Cell0 R_a 4 = 42 Cell0 R_a 5 = 42 Cell0 R_a 6 = 45 Cell0 R_a 7 = 48 Cell0 R_a 8 = 49 Cell0 R_a 9 = 52 Cell0 R_a 10 = 56 Cell0 R_a 11 = 64 Cell0 R_a 12 = 74 Cell0 R_a 13 = 128 Cell0 R_a 14 = 378 [R_a0x(Ra Table)] xCell0 R_a flag = FFFF xCell0 R_a 0 = 38 xCell0 R_a 1 = 41 xCell0 R_a 2 = 43 xCell0 R_a 3 = 44 xCell0 R_a 4 = 42 xCell0 R_a 5 = 42 xCell0 R_a 6 = 45 xCell0 R_a 7 = 48 xCell0 R_a 8 = 49 xCell0 R_a 9 = 52 xCell0 R_a 10 = 56 xCell0 R_a 11 = 64 xCell0 R_a 12 = 74 xCell0 R_a 13 = 128 xCell0 R_a 14 = 378 [Data(Calibration)] CC Gain = 10.204 CC Delta = 10.184 CC Offset = -0.71 Board Offset = -1.2 Int Temp Offset = 0.0 Ext Temp Offset = 0.0 Voltage Divider = 18709 [Current(Calibration)] Deadband = 5 [Codes(Security)] Sealed to Unsealed = 36720414 Unsealed to Full = FFFFFFFF Authen Key3 = 01234567 Authen Key2 = 89ABCDEF Authen Key1 = FEDCBA98 Authen Key0 = 76543210