Hallo
I'm considering to use the LM5116 in my design. The specs for normal operation are:
Vin: 60..75V
Vout: 12 V
How ever, I wonder how the LM5116 works for Vin < Voff,nom (=12 V). (only appears in fault cases)
My assumtion is that the LM5116 operates at max duty cycle, which is a limited by the switching frequency and the minimum off time.
Is it possible to clamp the Vout to Vin for that case by using the UVLO and a Pull-up resistor for the high switch?
(The aim is to keep Vout as high as possible if Vout<12V)
Thank you for your help!
Simon