Hi,
I'm designing a board with 6 TPS54620's driving LED modules. Input is 36 volts and output will be 25 or 27 volts or so at 50 watts. I'm switching down at 200KHz. I don't want beat notes whining, so I want to sync them. I wondered if I could set one with a resistor on the RT pin, than divide the phase node voltage down to the next RT pin. I could even load it with a bit of capacitance so it switches a little later and end up with all 6 parts synced out of phase. My duty ratio will be around 70 or 75%, so it'll be a valid wave form.
1. Is running the phase node around on a trace going to cause EMI trouble?
2. Will the PLL's behave? I can imagine the 6th part in the chain having issues.
3.Should I bite the bullet and put a micro on the board?
4.Are the beat notes likely to be audible any way?
Thanks