Can you please help me find an upgraded solution to the BQ24032A.
We are currently using the bq24032A in a design, but are upgrading the
battery to a 3.7V 5200mAh pack. Can you please recommend a higher charging current power path part that also has a USB power input? I was looking at the bq24170, which does not support a USB input, but we could
always diode-OR with the AC input.
The BQ24295 doesn't seem to fit as it does not have an AC power path input
The BQ24618 seems to have the pieces but pretty much has everything outside; looking for more integration if possible.
Li Ion
single cell
powerpath
USB
greater than 1.5A charging
Thank you,
Adam