Other Parts Discussed in Thread: LMR14203
Hello!
I use the LMR14203 in SOT23 with following values:
Vin 36V, Vout 10V, Iout 150mA max.
In datasheet is to see a 15uH value for inductor, but in simulation it's 150uH. All suggested other values for the inductor are between 125uH and 330uH. Also, the EvalBoard shows a 15uH inductor, too.
So my question is, what is correct, the 15uH value, or the 150uH value from Webbench?
Thank you!
Jurgen.