Hi all
I have a TPS61030 application that utilizes 3 nos of AA size cells (1.5V each) and a current limiting front-end at the output that supplies a steady (but user-selectable) current option of either 500mA or 1.0A.
The circuit works well but the cells start heating up after some time while on continuous discharge and then actual supply current drops till the device locks up (typically in an hour or so). The issue is the same with ordinary Zinc-chloride cells or heavy duty Alkaline cells. I haven't tested with NiMH or NiCD cells yet.
Any pointers to this would be greatly appreciated.
At the moment i have thought of hooking up a simple timer that alternately switches on a low RDSon NMos device connecting to two different battery packs so that the supply can remain steady while one battery pack can cool-off while the other discharges and then switch over, perhaps in half-hour cycles. But this is going to be a clunky solution which i would preferably like to avoid.
Thanks and regards
Soumitra