Trying to use the TPS2540 in CDP mode via the EVM. The EVm is plugged into a host computer (laptop) through J2 and a power supply through J1. There is a tablet PC connected to J3A and a resistive load connected to J3B. What is being seen on the output for charging is that the current is no more than 500mA. It seems like the part is being operated in SCP just because of the current limit of 500mA. Of course, the resistive load will only see 500mA, but the tablet PC should definitely see more than 500mA.
The datasheet shows that there is a two step process for negotiation between the portable device and the TPS2540. So how does the PC connected to J2 interaction within this negotiation process to know what current limit should be set? Woudl the data line voltage levels correspond to this? Also, if there is addition power available at J1, how does that affect how much current is present to the portable devices.
What wuold you recommend on determining if the TPS2540is running in CDP mode? Checking the D+ and D- lines for the correct voltages during the negotiation process?