This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS73701 ahd TPS78222 Question

Hello.

1  TPS73701

①  OUT pin  GND Short
   What happens to operation of this device?
② EN pin open.
    What happens to operation of this device?
③ FB  pin open.
  What happens to operation of this device?

2  TPS78222
①  OUT pin  GND Short
   What happens to operation of this device?
② EN pin open.
    What happens to operation of this device?

Thank you for your consideration.

 

 

  • Hi Masazumi,

    TPS73701

    1. OUT shorted to GND:
      1. The device will go into current limit.  Please see the datasheet for information on the current limit.  Particularly look at Figures 12, 13, and 14.
    2. EN pin Open:
      1. The EN pin is floating.  If the voltage on EN goes above the EN pin high threshold, the device will turn on, otherwise it will remain off.  As EN is floating, the device could alternate between off and on states.
    3. FB pin open:
      1. Again as the pin is considered floating, it will depend on the actual voltage on the pin.  Most likely the device will follow Vin similar to during start-up.

    TPS7822

    1. OUT shorted to GND:
      1. The device will go into current limit.  Please see the datasheet for information on the current limit.  Particularly look at Figure 9.
    2. EN pin Open:
      1. The EN pin is floating.  If the voltage on EN goes above the EN pin high threshold, the device will turn on, otherwise it will remain off.  As EN is floating, the device could alternate between off and on states.

    Very Respectfully,

    Ryan