This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24192i minimum Sys Out in battery mode

Other Parts Discussed in Thread: BQ24192I

Hi,

We are planning to use BQ24192i in one of our design and using a Single cell battery in system. We are feeding the output of BQ24192i (VSYS) to input of Power Management chip  which has input range 3.5V-5.5V.

In scenario when  system is working only on battery( No input at VBUS) .If Battery voltage goes below 3.5V . ( For example 2.8V-3.4V) what will be the VSYS output .

1.  Will It cut off the power if battery voltage goes below 3.5V

2.  Will it follow the Battery voltage as there is no boost circuit shown in block diagram

3.  Or still it can provide 3.5V till some level.

4. What is the minimum battery voltage for which BQ24192i can provide 3.5V-4.2V at output .

 

Thanks & Regards,

Bhupendar