Dear PMU team,
I'd like to power an OMAP-L138 based design through the TPS65070. The system is powered by a 12V battery. From the data sheet it is not quite clear whether I can connect the 12V supply directly to the AC pin converting internally to a 5-6V VSYS which in turn can be used to input to VINDCDC and VINLDO. Would this be possible, or do I need to convert the 12V to 5V externally with an additional DC/DC converter to power the TPS65070?
Any clarification would be highly appreciated.
Best Regards
Hans