Hi,
I have a big problem ! I use TPS5430 to transfer 12 to 24Vdc input power to 5.0 Vdc output.
Everything is fine when my system operating at 85C high temperature environment in chamber box.
Even wide temperature cycle test from -40C to 85C that our system continue operating.
But TPS5430 can't cold boot up to generate 5.0 Vdc, when I shutdown sytem with turn off power source and waiting 1 ~ 2 hours then turn on the power source (12 to 24Vdc)
The circuit design on ENA pin is floating, and TPS5430 should be start up even if -40C low temperature environment.
Anyone can help me ?