Hello,
I can't find the load regulation parameter of the TPS62080A.
There is load regulation for fixed voltage version only.
TPS62080A has Vfb parameter and the figure of "Output Voltage vs Load Current", but not load regulation.
There is load regulation for fixed voltage version only.
TPS62080A has Vfb parameter and the figure of "Output Voltage vs Load Current", but not load regulation.
(1)
Vfb parameter is specified on the full temp range and full current range?
If we don't consider tolerance of resistor, we can calculate output voltage acuracy by Vfb only?
Vfb parameter is specified on the full temp range and full current range?
If we don't consider tolerance of resistor, we can calculate output voltage acuracy by Vfb only?
(2)
Are below my understanding correct ?
Vfb:0.438V(min) is specified at the condition of Ta=-40°C and Iout=0mA ?
Vfb:0.462V(max) is specified at the condition of Ta=85°C and Iout=1.2A ?
Vfb:0.45V(typ) is specified at the condition of Ta=25°C and Iout=0mA ?
Vfb:0.462V(max) is specified at the condition of Ta=85°C and Iout=1.2A ?
Vfb:0.45V(typ) is specified at the condition of Ta=25°C and Iout=0mA ?
Best Regards,
Ryuji Asaka
Ryuji Asaka