I have a question regarding the UVLO feature of the LM5122 EVM. When I pull UVLO to GND, I expected the controller shut down as the datasheet indicates and Vout should be 0V. But on my test, Vout is almost same as Vin. The high side switch is always on. I tried different modes, the results are the same. I want to use the UVLO as the on/off control pin, but it seems not working that way. Can you please explain?