Hi
I want to use TPS7A5433 in my design. Input voltage is12V and out put is 3.3V, 1.5A current. As per thermal calculation in TI Tjuncation temperature is going at 982.5 degree Celsius.
As per calculation
Power Dissipation (Pd) = (Vin-Vout) x I load
= (12-3.3)V x1.5A
= 13.5W
Temperature rise by LDO due to its own dissipation
Trise = ΘJA x Pd
= 50.5degC/W x 13.5W
= 681.75degree C
As per calculation I can use this LDO if load current is less than 0.2A, am I right?
Which calculation base part provide 1.5A load current?
Would you please answer my query and guide me?
Also answer I can go with this part in my design.
Regards,
Ravi