This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

NEED INFORMATION- TLV431BQDBZTG4

Hi Can you please provide the following information for the TLV431BQDBZTG4 Part ?

1. Junction Temperature Max (Tj Max)

 2. Typical Power dissipation (Pd typ)

3. Maximum Power dissipation (Pd max)

4. Thermal Resistance Junction to Ambient (Theta JA

5. Thermal Resistance Junction to Board (Theta JB)

6. Thermal Resistance Junction to Case (Theta JC)

7. Weight

 

  • Jayakumara,

    1) 150C
    2) Pd set by application, cathode voltage multiplied by cathode current, VKA*IKA. (1.25mW with VKA=1.25V, IKA=1mA)
    3) Max Pd is maximum VKA * maximum IKA, 6V * 15mA = 90mW (also limited by Tj)
    4) TJA = 206C/W
    5) not found
    6) not found
    7) 18.3mg