Hi,
I am presently using UCC2946 with a capacitor at pin WP of 680pF. I observe that the WDO remains high while WDI is statically driven to 0V through a 10K pull-down resistor. This indicates that the watchdog is disabled. I suspect that 10K is too high, but the datasheet of the UCC2946 does not indicate the maximum value of the output resistance of the circuit driving the WDI pin. Is it possible to indicate what would be that maximum value?
Thanks
Amir