This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Input/Output capacitor at TLE4275 and TL720M05



Hi

Would you tell be input/output capacitor at below device.

・TLE4275QKVURQ1

・TL720M05QKVURQ1
 
Question 1
Can I use seramic capacitor at input?
 
I checked APN, this schematic use to 22uF, so I think answer is yes.
 
Question 2
Can I use seramic capacitor at output?
 
Data sheet only below information.
More than 22uF
Less than 5Ω
 
Best regards,
 
masa