Hi,
I am having problem in Battery Charger functionality. I have attached my circuit. Below are my observation:
Battery Voltage: 3.7V (Single Cell)
VREF: 3.79V (Pin 12)
OVPSET (Pin 18): 0.65V
AC_SET(Pin17): 1.52V
AVCC (Pin 4): 5.0V
ISET (Pin13): 0.45V
TS (pin 10): 1.75V
PVCC(Pin2 &3): 4.5V
REGN (Pin20) : 0.10V
SRP (Pin15) : 3.8V
SRN (Pin 16): 3.8V
BTST (Pin21) : 3.54V
SW(Pin1 &24): 3.8V
BATDRV(pin19): 4.54V (Not used in the design, Testpoint)
TTC (Pin11) : 0.5V
All the above voltages are with Ground reference.
I am very new to Battery charger and not sure why the Charging is not taking place.
I am not able to understand why the REGN is not in right level and also VREF pin is 3.8V not 3.3V
Thank you for your kind attention and immediate response.
Sincerely,
Rajendra..