We have an application that uses the TPS79333DBVR to regulate the power to a CPU. This product comes in to flavors, one using the TPS79333DBVR to regulate the voltage and another that gets its power from and external source. The question I have is on the externally powered unit.
In the externally powered unit the TPS79333DBVR is omitted and and Vcc is connected to the other power source. The problem this causes is that we have to stock two different versions of our product. If we leave the TPS79333DBVR on the board and not even power it up would allow us to have only one unit simplifying our inventory.
The question is what harm could this do to an unpowered TPS79333DBVR? The voltage output and the extern power voltage are the same, but if this might cause a failure of the TPS79333DBVR we would have failures in the field. So how much external voltage can the Vout output take in the unpowered state and if it fails what is the failure modality? If it fails open it wouldn't affect us, but if it fails as a short that's a big problem. So how much overvoltage can the Vout take before it fails?
Thanks
Paul