This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Current problem about LM5022

Other Parts Discussed in Thread: LM5022

Hello TI:

    I used WEBENCH to design a 10~16V input, 12V/5A output DC/DC circuit. In the case, I got Rsns=0.02Ohm for the current limit. Actually, on my board, I measured 6A @ 10V input and 7A @ 16V input and it got huge current when output short (10A @ 10V, 14A @ 16V).

Can I reduce current via changing other parts such as inductor, capacitor, MOS, Rt etc.?