This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3464 DIM pin

Expert 7280 points


Dear all,

Could you confirm me that this would be safe to permanently link the DIM pin (PIN #2) to the VCC output (PIN 13, 6.51Vout max) ?

Only the absolute maximum ratings are specified for this PIN, which indicates 7V.

I guess the input current of this pin is very low, so we can still use a ~100k total resistsor divider to set a ~4 to 5V level for this input.

Thanks a lot for your inputs !

Best regards,

Pierre-Alexandre