Other Parts Discussed in Thread: LMZ22003, LMZ22008
Hello,
I am working with a design that is migrating from the LMZ22008 to the LMZ22003. The issue is that the LMZ22008 was capable of running at lower frequencies down to 350kHz which made using a 500kHz sync signal a viable design choice.
However the move to the LMZ22003 with its minimum sync frequency of 650kHz I wanted to check if supplying a 500kHz sync signal would cause instability by not being within the designed range or if there is a potential that the converter will shut off in the case a longer duty cycle pulse at 500kHz based on the discussion on the bottom of Pg. 19 of the datasheet.
Thank you for your help.
Ryan May