This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP2989 error flag / current limiter?

Other Parts Discussed in Thread: TMS320F28335, LP2989, ISO721

Hello,

Is there any need for a current limiter resistor between LP2989AIM-5.0/NOPB ERROR pin and a DSP?

Haven't seen this in datasheet.

Thank you.

  • All depends how much current the DSP pin can source when pulled low by the ERROR pin.

    Datasheet suggests that the ERROR pin not sink more than 150uA, otherwise a low level on the ERROR pin may not be low enough.

  • Hello Donald,

    Thank you for the reply.

    I am not sure I am following up how these sentences join to a result.

    DSP is TMS320f28335 (Experimenter Kit). 28335 and I believe most or all DSP's can provide up to 150uA in any IO pin. So if this is the max. current value that the LP2989 comparator sinks when low, I believe there is no reason to check on that - am I missing anything?

    Now, what I found in the datasheet is the "Condition" Io(COMP) = 150uA for Output LOW Voltage. I am particularly not sure if this is the measurement condition (it seems to be) or a real limiter present in the chip circuit, ie, it will never sink/source any more than that. So, can you please tell me if a need a current limiting resistor interfacing and what is its recommended value.

    The actual signal chain is LP2989 Error Pin -> ADG732 (MUX) -> ISO721 (+5V/+3.3V) -> 28335 (DSP).

    Thank you,

    Thiago

  • There is no active current limit, per se.

    The resulting voltage is a function of the collector-emitter saturation for the NPN transitor that pulls the pin low.

    You can sink more current, but the resulting voltage is higher.