This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCD9012x Brownout Function

I am looking at this feature and just wanted to verify that the requirement to use this is as follows:

Hold up the 3.3V rail as it drops from 2.9V to 2.6V for 5mS with an 80mA current draw.

This would take a minimum of 1,400uF.  Is this correct or am I missing something?

Shawn