Sir,
Any digital power device can support below spec?
Non-Isolated DC/DC
Vin: 40V
Vout1 adjust from 8V ~ 35V/1A
Vout2 adjust from -8V~-35V/1A
Regards,
Derek Lee
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.